:CHSCanner[:SENSe]:POWer[:RF]:EXFActor <num>

(Read-Write) Set and query the extrapolation factor in dB.

Relevant Modes

Channel Scanner

Parameters

 

<num/char>

Extrapolation factor value in dB.

MINimum: -100 dB

MAXimum: 100 dB

This command accept DEFault, MINimum and MAXimum as arguments

Examples

:CHSC:POW:EXFA 15 */Sets the extrapolation factor to 15 dB

Query Syntax

:CHSC:POW:EXFA? */queries the extrapolation factor value

Return Type

numeric

Default

0


Last Modified:

26mar2024

New command (A.13.00)